livre blanc

Machine Learning at the Edge: Using HLS to Optimize Power and Performance

Machine Learning at the Edge: Using HLS to Optimize Power and Performance

Moving machine learning to the edge has critical requirements on power and performance. Using off-the-shelf solutions is not practical. CPUs are too slow, GPUs/TPUs are expensive and consume too much power, and even generic machine learning accelerators can be overbuilt and are not optimal for power. In this paper, learn about creating new power/memory efficient hardware architectures to meet next-generation machine learning hardware demands at the edge.

Partager

Ressources associées

Réduire la probabilité d'erreur de conception de 25 %
Case Study

Réduire la probabilité d'erreur de conception de 25 %

Le groupe Carraro utilise VeSys pour réduire de moitié le temps consacré aux essais fonctionnels...