白皮书

Expanding the scope of Mixed-Signal Verification with Symphony Mixed-Signal Platform

Expanding the Scope of Mixed-Signal Verification with Symphony Mixed-Signal Platform

The number of mixed-signal interactions and the complexity of the feedback loops on ICs is increasing which makes verifying them a difficult and error prone task. Verification teams have traditionally used mixed signal simulations with relaxed accuracy settings for the analog portion as part of their functional verification flows at the top level and subsystem level to achieve good performance with the goal to catch primarily errors in A/D (analog/digital) connectivity and interfaces. Many errors that result from realistic analog block behavior which can affect digital blocks through A/D feedback go undetected in relaxed accuracy simulations thereby causing chip failures. Symphony Mixed-Signal Platform delivers the accuracy needed with fast mixed-signal simulation performance to be able to catch the errors resulting from the realistic behavior of analog blocks and A/D feedback.

分享

相关资源

 用 CFD 仿真支持您的设计流程
Video

用 CFD 仿真支持您的设计流程

使用 Simcenter FloEFD 进行 CFD 仿真

Using fast CFD simulation to improve drag and vehicle aerodynamics
Webinar

Using fast CFD simulation to improve drag and vehicle aerodynamics

Understand how to use state-of-the-art CFD simulation with rapid turn-around time to optimize drag and vehicle aerodynamics.