电子书

车间数字化制造主管指南

车间数字化制造主管指南。汲取零件制造主管的见解。

当今世界的主管精英们都敏锐地意识到,数字化是制造业的未来。数字化制造也已经成为解决复杂的生产问题和改进机械车间业务的关键。


数字化制造有助于促成创新产品设计和最佳性能的完美结合。拥抱数字化制造的企业必然可以:

  • 加速产品上市
  • 降低风险
  • 增加利润
  • 提高市场地位

在本电子书中,您可以了解到当下零件制造业面临的升级挑战,并掌握机械车间是如何凭借数字化制造的力量应对挑战的方法。

汲取零件制造主管应对此类挑战的经验

电子书摘录:

作为一家总部位于德国的汽车供应商,EDAG 集团发现,实施新型仿生设计和增材制造技术,不会耽误上市时间。EDAG 的目标是抓住汽车电气化提供的契机,保持行业竞争优势。

数字孪生赋能 EDAG 在统一的软件生态系统中进行创成式工程设计、仿真和 3D 打印制备。其可见性成果为削减设计时间可达50%。

“我们证实了增材制造也适用于大规模生产,成功解决了汽车行业面临的实际挑战。” -- 塞巴斯蒂安·弗留格尔 (Sebastian Flügel),EDAG Scalebat 项目负责人

使用同一解决方案进行零件制造的优势

得益于西门子公司 NX 软件提供的集成式软件,从数字化零件模型到成品实现了无缝制造,让零件制造达到前所未有的简单水平。

NX 助您利用一个全面的软件实现零件制造的转型,以便能够对 CNC 机床进行编程,控制机器人单元,驱动 3D 打印机以及监控产品质量。贵公司这样的零件制造商可以使用高级功能和集成式仿真工具实现编程自动化,同时联通端到端零件制造流程。

创新模具制造商 iMFLUX 通过数字化制造引领前沿

iMFLUX 是一家模具制造企业,为其先进的车间集成了颠覆性的软件和机器学习功能。NX 软件帮助 iMFLUX 加快其模具设计到制造流程,提高了零件质量、降低了成本并缩短了企业交付时间。

自从采用 NX 和 Teamcenter 软件以来,iMFLUX 体会到自动化模具极大提高生产率的过程,并且可以捕获、优化和重用企业知识。该公司已经享受到无缝生产过程中的人员、系统和资源的联通。西门子软件允许 iMFLUX 制造主管灵活运营,通过数字化制造让公司在当下满足未来的需求。

分享

相关资源

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification
Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP
Webinar

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP

STMicro presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) and a method to add constraints to the random values generated in UVMF.

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation
Webinar

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?
Webinar

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?

Discover how C++ & SystemC/MatchLib HLS is more than just converting SystemC to RTL. In the RTL Design space, we will cover our technology for Power Optimization with PowerPro Designer & Optimizer.

Alibaba: Innovating Agile Hardware Development with Catapult HLS
Webinar

Alibaba: Innovating Agile Hardware Development with Catapult HLS

At the IP level, an ISP was created within a year using Catapult, a task impossible using traditional RTL. To reduce dependency on designer experience, Alibaba introduced an AI-assisted DSE tool.

Space Codesign High-Level Synthesis for Hardware/Software Architectural Exploration of an Inferencing Algorithm
Webinar

Space Codesign High-Level Synthesis for Hardware/Software Architectural Exploration of an Inferencing Algorithm

Space Codesign Seminar: design flow including HW/SW co-design & HLS that allows developers to migrate compute intensive functions from software running on an embedded processor to a hardware based accelerator.