电子书

用于能源系统运营的物联网能源管理

在发电厂内爬梯子的人。

能源企业面临市场波动、脱碳和地缘政治动荡的干扰。为了增加收入,企业必须提高运营效率,同时拥抱可持续性和创新。

下载我们的电子书,了解优质运营方法如何实现:

  • 使用工业物联网(IoT)能源管理平台连通工厂、系统和资产
  • 在数字孪生中实现连续的闭环反馈
  • 优化能源系统运营

提高电厂性能和生产力水平

通过为现场操作员提供高度定制化应用程序,在操作问题发生之前提醒他们,从而提高发电厂性能。应用实时性能分析对关键系统进行故障排除,模拟新概念或诊断可能导致不稳定性或工厂停机的内部流程问题。阅读我们的电子书,了解如何在整个企业中实现优质运营!

使用能源预测分析软件做出更好的决策

数字化可帮助企业减少排放并实现优质运营。使用高级能源预测分析技术,贵公司可以:

  • 做出更周全的决策
  • 分析大型数据集
  • 发掘趋势
  • 预测需求

下载电子书,了解如何加速企业的数据驱动型未来。

分享

相关资源

Xperi®: A Designer’s Life with HLS
Webinar

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection th

High-Level Synthesis Verification Technologies and Techniques
Webinar

High-Level Synthesis Verification Technologies and Techniques

This session will describe applying known and trusted static, formal and dynamic approaches to verification performed at the C++ or SystemC HLS level of abstraction.

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques
Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations.