电子书

加快电子行业的数字化转型

通过增强的协作流程和创新来优化产品开发

以数字方式实现全球连接

了解电子企业如何利用数字化转型以更快的速度和更低的成本开发优化的产品。本电子书探讨了一个经过验证的五步式框架,可帮助企业评估其数字化成熟度并加速迈向全面优化的闭环企业。

实现数字化成熟度的 5 个步骤

在当今快速发展的电子行业中,企业面临着越来越大的压力,他们需要提供更复杂、更智能的产品,同时保持质量并加快上市时间。这份全面的指南探讨了数字化转型如何通过增强协作、简化流程和持续创新来帮助企业克服这些挑战。

数字化转型不仅仅是将手动流程数字化,它还从根本上重新构想团队的协同工作方式和产品开发方式。通过我们的五步式框架,企业可以评估其数字化成熟度,并系统地将其运营从基于文档的系统转变为利用数字孪生、人工智能和自动化功能实现的完全数字化工程流程。

分享

相关资源

Xperi®: A Designer’s Life with HLS
Webinar

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection th

High-Level Synthesis Verification Technologies and Techniques
Webinar

High-Level Synthesis Verification Technologies and Techniques

This session will describe applying known and trusted static, formal and dynamic approaches to verification performed at the C++ or SystemC HLS level of abstraction.

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques
Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations.