Panoramica della soluzione

The future of ship design and engineering

Digital twin representation of an innovative propeller and rudder

The future of ship design and engineering is critical to shipbuilders. This phase of shipbuilding projects typically represents 5 to 10 percent of the overall production cost of a vessel, and yet has an impact on about 85 percent of the construction costs. It is also during this phase that ~90 percent of the vessel performance is determined.

In today’s uncertain market, getting your design right the first time is critical to ensure success. Can digital twin technology help make the ship design and engineering process more efficient?

Controlling the design spiral

Today, the ship design and engineering process is largely based on the design spiral. However this process is inefficient. Steps in the spiral typically involve independent functional teams, which results in collaboration bottlenecks and data silos. In addition, ships today are a lot more complex than they were when the design spiral was first introduced. To manage today’s complexity and stay afloat in an increasingly competitive market, adopting an integrated approach to ship design and engineering is not an option, it is a necessity.

Integrated ship design software

Adopting an integrated ship design software enables shipbuilders to remain in control of the design spiral. Bring multi-discipline design processes into a centralized environment, to enable globally distributed teams to work with a common set of data, tools and processes. Increase overall project efficiency and improving business agility by breaking down silos of information. A fully integrated solution that enables seamless process execution from initial design to detail and production design is in your future of shipbuilding and design.

More in the series:

Condividi

Risorse correlate

Il calcolatore ROI del PLM prevede il ritorno sull'investimento
Analyst Report

Il calcolatore ROI del PLM prevede il ritorno sull'investimento

Scopri in che modo il software di gestione del ciclo di vita del prodotto si ripaga da solo migliorando le prestazioni di progettazione e ingegneria. Misura il ritorno sull'investimento della gestione PLM.

White paper gratuito sul software PDM: Funzionalità e vantaggi principali
White Paper

White paper gratuito sul software PDM: Funzionalità e vantaggi principali

White paper gratuito sul software PDM! Scopri le principali funzionalità e i vantaggi chiave di un sistema PDM per migliorare la produttività nella tua azienda!

Le migliori strategie PLM per soddisfare i requisiti di prodotto e rispettare i termini di consegna
E-book

Le migliori strategie PLM per soddisfare i requisiti di prodotto e rispettare i termini di consegna

Scopri come le aziende leader dello sviluppo prodotto hanno risolto le principali sfide del settore - Soddisfare i requisiti di prodotto (53%) e rispettare i tempi di consegna (45%) - con le cinque strategie illustrate in ...

Migliorare le prestazioni di sviluppo prodotto con una gestione efficace dei dati
E-book

Migliorare le prestazioni di sviluppo prodotto con una gestione efficace dei dati

Leggi l’eBook per conoscere le best practice di gestione dei dati di prodotto adottate dalle aziende leader che progettano, ingegnerizzano e/o fabbricano prodotti