descripción general de tecnología

Semi-trunk routing

Tiempo estimado de visualización: 2 minutos

This capability allows the user to create a Sketch plan that will only be routed on one end of the plan. By choosing the new command, Route Semi-Trunk, the Sketch plan will be optimized for the end opposite the Route to Dot, and then routed.

This can help the user to pre-route interfaces that may still require placement or pin and gate swapping optimization. To complete optimization of an FPGA or ASIC, and insure the placement of the interface is complete, the user can easily Reverse the Sketch plan to optimize the other end.

Learn more on Design Automation.

Compartir

Recursos relacionados

Toma la vía rápida con Teamcenter X SaaS PLM
Video

Toma la vía rápida con Teamcenter X SaaS PLM

Echa un vistazo al software como servicio de la gestión del ciclo de vida del producto (SaaS PLM), fácil de acceder y utilizar.