white paper

Expanding the scope of Mixed-Signal Verification with Symphony Mixed-Signal Platform

Expanding the Scope of Mixed-Signal Verification with Symphony Mixed-Signal Platform

The number of mixed-signal interactions and the complexity of the feedback loops on ICs is increasing which makes verifying them a difficult and error prone task. Verification teams have traditionally used mixed signal simulations with relaxed accuracy settings for the analog portion as part of their functional verification flows at the top level and subsystem level to achieve good performance with the goal to catch primarily errors in A/D (analog/digital) connectivity and interfaces. Many errors that result from realistic analog block behavior which can affect digital blocks through A/D feedback go undetected in relaxed accuracy simulations thereby causing chip failures. Symphony Mixed-Signal Platform delivers the accuracy needed with fast mixed-signal simulation performance to be able to catch the errors resulting from the realistic behavior of analog blocks and A/D feedback.

Share

Related resources

Symphony Mixed-Signal Platform
Fact Sheet

Symphony Mixed-Signal Platform

Symphony Mixed-Signal Platform is the industry’s fastest and most configurable mixed-signal solution to accurately

Mixed-signal verification of an EESY-IC high-speed ADC with Symphony
White Paper

Mixed-signal verification of an EESY-IC high-speed ADC with Symphony

The Symphony Mixed-Signal Verification Platform allows EESY-IC to verify full-chip, mixed-signal designs in a few hours with desired accuracy, providing them more than 10 times the productivity than their previous flow.

Simplifying Mixed-Signal Verification with the Symphony Platform
White Paper

Simplifying Mixed-Signal Verification with the Symphony Platform

This paper explores the potential shortcomings of legacy mixed-signal verification tools and methodologies for AI, automotive, IoT, communication, and industrial hardware applications.