This paper presents the research findings and application results of the ML-Statistics Risk Pattern Predictor (ML-SRPP), a novel approach that combines pattern segmentation, Greedy algorithm-based sampling, and unbiased statistical estimation to predict and mitigate process-related defects in advanced semiconductor technology nodes.
The ML-SRPP framework first extracts the pattern type and usage frequency of the product design using a pattern segmentation technique, then applies the Greedy algorithm to select the most representative patterns within the measurement constraints. An unbiased estimation method is used to ensure 99% reliable process variation data, which is then incorporated into the ML model.
The enhanced ML-SRPP model can predict the statistical risk of critical patterns, identifying the minimum and maximum critical dimension (CD) values that patterns can exhibit. This capability enables early detection and mitigation of potential defects related to CONTACT, VIA, and metal layers, contributing to significant yield improvements in the latest 3nm products.
The paper demonstrates the effectiveness of the ML-SRPP approach through several case studies, including CONTACT_A open risk, VIA_A not open/short risks, CONTACT_B short risks, and VIA_B to METAL_A short risk prediction and prevention. The methodology has been applied to 2 nm and 1.4 nm technology nodes, showcasing its scalability and importance for advanced semiconductor development.
This paper was presented at the 2025 SPIE Advanced Lithography + Patterning symposium.