电子书

借助产品设计技术大规模提速

展示连通性的重型装备机器内部

对于生产相对较小的批量就需要大量工程工作的行业而言,上市时间是主要设计推动因素。贵公司是否在紧随定制化需求的同时仍能按时交付设备?

下载我们新推出的此电子书,了解如何借助产品设计技术大规模提速,从而帮助应对如今独特的重型装备市场中的复杂性。

降低成本并缩短上市时间

复杂性、法规合规需求的增加以及对于定制化和本地化设计变体需求的增加,都可能让项目减慢。积极对抗的时候到了。不妨部署相关工具和流程,帮助降低成本并缩短上市时间,这是影响盈亏底线的两个关键因素。包括仿真和验证管理在内的统一协同式环境可以帮助所有类型的设计降低成本并缩短上市时间。

多学科设计可以赋能实现跨团队协同

如今出现的大部分创新都需要机械、电子和软件领域紧密合作。对于装备设计而言,这就意味着设计流程将涉及更多参数、更多实体和更多利益相关者。多学科设计方法可以赋能实现跨团队协同,通过避免无穷无尽的设计迭代来提高效率。

持续验证

可靠性的提高以及风险的降低也可以通过持续验证和确认来实现。需要设计流程来推动通用性和重用性,从而赋能实现不同设计变体的虚拟验证和确认。

下载我们新推出的此电子书,详细了解如何在变体和复杂性增加的情况下仍能加快装备设计。

分享

相关资源

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification
Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP
Webinar

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP

STMicro presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) and a method to add constraints to the random values generated in UVMF.

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation
Webinar

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?
Webinar

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?

Discover how C++ & SystemC/MatchLib HLS is more than just converting SystemC to RTL. In the RTL Design space, we will cover our technology for Power Optimization with PowerPro Designer & Optimizer.

Alibaba: Innovating Agile Hardware Development with Catapult HLS
Webinar

Alibaba: Innovating Agile Hardware Development with Catapult HLS

At the IP level, an ISP was created within a year using Catapult, a task impossible using traditional RTL. To reduce dependency on designer experience, Alibaba introduced an AI-assisted DSE tool.

Space Codesign High-Level Synthesis for Hardware/Software Architectural Exploration of an Inferencing Algorithm
Webinar

Space Codesign High-Level Synthesis for Hardware/Software Architectural Exploration of an Inferencing Algorithm

Space Codesign Seminar: design flow including HW/SW co-design & HLS that allows developers to migrate compute intensive functions from software running on an embedded processor to a hardware based accelerator.