电子书

部署多学科设计方法以加快设计

田野中的重型装备机械

在当今的重型装备中,创新往往会增加机械、电气和软件之间的交互并加剧复杂性。如果企业的各个团队彼此脱节,使用自己的工具和流程在孤岛中工作,那么企业将无法应对此复杂性。制造商可以通过部署集成式的多学科方法来解决此问题,因为该方法支持机械、电子和软件的同步设计。

请下载这本新的电子书,详细了解重型装备制造商如何加快设计创新型装备并保持竞争优势。

融合电气设计软件和机械设计软件

在重型装备机械中,电气化等创新增加了机械和电气组件之间的交互,需要相应的设计团队展开紧密协作。电气设计软件和机械设计软件必须融入同一环境中,并能共同访问共享的数据。这样它们能够考虑彼此的设计决策并同步展开工作。例如,它们可以将模型视图从一个工具同步应用到另一个工具,同时提高两者的生产效率。

利用 CAD 软件创建仿真模型

作为集成式软件方法的一部分,必须在设计的工程端优化多学科性能。这要求计算机辅助设计 (CAD) 软件平台具备仿真功能,可从分析的各个性能方面提供所有相关的物理特性并加以综合利用。通过在 CAD 中提供此类功能并保持关联性,设计工程师就能够在流程早期获得合适的工具来帮助制定决策,否则决策只能在较晚的阶段做出。

请立即阅读这本新的电子书,详细了解面向重型装备制造商的这一简单、易于访问且灵活的端到端多学科设计方法

分享

相关资源

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation
Webinar

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis
Webinar

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis

Infineon & Coseda present on the adoption of High-Level-Synthesis at an existing SystemC system level model.

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification
Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP
Webinar

STMicroelectronics: A Common C++ and UVM Verification Flow of High-Level IP

STMicro presents a unified way to integrate the definition of RTL and C functional coverage and assertion (reducing the coding effort) and a method to add constraints to the random values generated in UVMF.

Alibaba: Innovating Agile Hardware Development with Catapult HLS
Webinar

Alibaba: Innovating Agile Hardware Development with Catapult HLS

At the IP level, an ISP was created within a year using Catapult, a task impossible using traditional RTL. To reduce dependency on designer experience, Alibaba introduced an AI-assisted DSE tool.