宣传册

Cybersecurity for machine builders

Industrial cybersecurity protects connected machines and systems against rising cyber threats. Siemens promotes a holistic, standards-based approach with multi-layered defense, secure design, and continuous risk management.

Cybersecurity for machine builders

Industrial cybersecurity has become a critical priority as manufacturing environments continue to evolve through digitalization, automation, and increased connectivity. The integration of operational technology (OT) with IT systems and cloud-based infrastructures has significantly expanded attack surfaces, exposing industrial systems to a growing number of cyber threats. Statistics show that smart factories are frequently targeted, with a high proportion of ransomware attacks affecting the manufacturing sector. This highlights an urgent need for comprehensive cybersecurity strategies that go beyond traditional IT protection and address the specific requirements of industrial environments.

At the same time, organizations face increasing regulatory pressure, particularly in Europe. Regulations such as the NIS2 Directive, the Machine Regulation, and the Cyber Resilience Act require companies to implement structured cybersecurity risk management, ensure product-level security, and meet lifecycle-based compliance obligations. These frameworks extend cybersecurity responsibilities across the entire value chain, from manufacturers and system integrators to end users. Failure to comply can result in financial penalties, operational disruptions, and reputational damage, making cybersecurity a key business and governance issue.

To address these challenges, Siemens promotes a holistic, end-to-end cybersecurity approach based on internationally recognized standards, particularly IEC 62443. This standard defines security requirements for all relevant stakeholders and covers the entire lifecycle of industrial systems, including secure product development, system integration, and operational management. By aligning with IEC 62443, organizations can create a consistent and scalable security framework that supports both regulatory compliance and operational resilience.

A central element of this approach is the “Defense in Depth” concept, which ensures multi-layered protection across all levels of an industrial environment. This includes physical security measures, plant-level controls, network security through segmentation and firewalls, and system-level protections such as patch management, authentication, and access control. The layered architecture reduces the likelihood of successful attacks and limits their impact by preventing a single point of failure.

Cybersecurity is not treated as a static solution but as a continuous management process. Organizations must regularly assess risks, implement organizational and technical measures, and continuously validate and improve their security posture. This iterative approach allows companies to adapt to new threats and maintain compliance with evolving standards and regulations. It also emphasizes the importance of awareness and accountability across all levels of the organization.

Siemens also integrates cybersecurity directly into its products through a secure-by-design philosophy. This includes features such as role-based access control, encrypted communication, secure boot processes, and digitally signed firmware updates to ensure system integrity and data protection. In addition, Siemens provides specialized solutions such as secure remote access platforms, industrial firewalls, and vulnerability scanning tools that enable companies to protect, monitor, and manage their industrial networks effectively.

Overall, the document demonstrates that effective industrial cybersecurity requires a comprehensive, lifecycle-oriented strategy that combines technology, standards, and organizational processes. By adopting a holistic approach, organizations can strengthen resilience, ensure regulatory compliance, protect critical infrastructure, and maintain long-term competitiveness in an increasingly connected industrial landscape.

分享