sách trắng

Making shift-left real: Why SystemC, MatchLib, and High-Level Synthesis are the right foundation for SoC design and verification in an age of AI

Top angle of a futuristic microprocessor chip

SoC teams are routinely told to “shift left”—to find design and verification problems earlier, where they are cheaper to fix—yet in most flows the first model that is both performance-accurate and authoritative is still the RTL, which arrives late and simulates slowly. This paper argues that SystemC models built with the open-source MatchLib library and synthesized with Catapult HLS close that gap. Such models exist early, simulate 30x–100x faster than RTL, are throughput-accurate with respect to the final implementation, and are the actual source from which the RTL is generated. Combined with a user-visible scheduling contract backed by formal proofs, they let most design, verification, and architectural exploration move to the source model. The same properties make this flow the natural foundation for the AI-driven design and verification flows now emerging.

Chia sẻ

Tài nguyên liên quan