приклад

Gaining a better understanding of the calendaring process to track areas and particles during compaction

Technical University of Munich uses Simcenter EDEM to optimize battery production

Technical University of Munich uses Simcenter EDEM to optimize battery production

Technical University of Munich

Technical University of Munich is one of Germany’s leading universities for research and teaching in natural sciences and engineering.

https://www.tum.de/en

Головний офіс:
Munich, Germany
Продукти:
Simcenter EDEM
Промисловий сектор:
Battery

Поширити

By coupling the Simcenter EDEM contact models, EEPA and bonded particle model, as well as their calibration on battery electrode materials, we can identify possible process parameters during calendering.
David Schreiner, Research Associate, Technical University of Munich

About the customer

The Battery Production Group at the Institute for Machine Tools and Industrial Management at the Technical University of Munich (TUM) researches the production of innovative battery cells. The core of the work is process development and the optimization of processes within battery production, from mixing, coating and calendering of the electrode materials to the formation of the final battery cells. All battery production steps are carried out in-house using the TUM’s electrode and battery production line.

Challenge

The performance of battery cells depends not only on the materials, but also on the composition and the microstructure of the electrodes. Each electrode material requires a new design of the manufacturing processes, which is why a deeper understanding of these processes is necessary. The TUM research group considers all aspects of electrode production from the handling of powdered active material to the finishing of electrodes, and includes research into processes such as mixing and dispersing, coating and drying, and calendering of the electrodes.

As the final step in electrode production, calendering is a critical process that significantly influences the mechanical and electrochemical properties of the electrode. To date, knowledge of the calendering process has been gathered at TUM with experiments. However, since the parameters of the calendering process have a significant influence on it, a profound understanding of the calendering process and its effects on the electrode is necessary. This includes process parameters such as roll temperature and speed, structural parameters (for instance, layer thickness and adhesive strength), and material and composition, as well as parameters of machine behavior (displacement and bending line).

A machine with cylindrical rollers has spheres falling.

The Technical University of Munich uses Simcenter EDEM to simulate the calendering process for lithium-ion batteries.

Our solution

With Simcenter™ EDEM™ software simulation, part of the Siemens Xcelerator business platform of software, hardware and services, the calendering process design can be enhanced to establish where potential calendering parameters can be identified and assessed using simulation. The concept for calendering process design encompasses three main modules: modeling of the electrode, parametrization of the electrode and identification of potential process parameters.

First, the input and output product of the calendering process, the electrode, is defined and then modeled. Therefore, based on the particle size distribution, density and thickness of the electrode, the control volume is defined and filled with particles. This is done by combining two contact models, Edinburgh-Elasto-Plastic-Adhesive (EEPA) and bonding. A verification of the electrode density and the particle distribution within the electrode concludes the model of the electrode. Since the composition of the electrode is variable, the sensitive simulation parameters of the modeled electrode are parameterized. To reduce the time and effort required for calendering settings, a tool for determining the calendering parameters has been developed.

“By coupling the Simcenter EDEM contact models, EEPA and bonded particle model, as well as their calibration on battery electrode materials, we can identify possible process parameters during calendaring,” says David Schreiner, research associate at TUM. “This provides additional value in the determination of parameters and helps us to gain an even better understanding of the calendering process, especially the possibility to track individual areas and particles during the compaction process.”

A dense grayscale cluster of particle-like structures varies in size.

Scanning electron microscope (SEM) image: NMC cathode from TU Munich, iwb, David Schreiner

Results

Comparing scanning electron microscope (SEM) images with Simcenter EDEM simulation images show the high degree of agreement with the Simcenter EDEM modeled electrodes. In addition, SEM close-up images of NMC particles show that the Nickel Manganese Cobalt (NMC) is embedded in the binder and carbon black matrix, confirming that the assumption of spherical particles is qualitatively verified.

The electrode to be simulated is composed of NMC622 active materials, conductive carbon black and binder. For this purpose, a constant particle size was assumed for the binder and the conductive carbon black, whereas for NMC a logarithmic normal distribution of the particle size was selected based on experimental measurements. In the simulation the electrode was generated by a dynamic factor into a representative control volume. The parameterization of the model is performed by pressure-displacement curves resulting from nanoindentation experiments.

The method was tested and verified against experiments that compared pressure-displacement response. Furthermore, sensitivity analyses of different parameters of the selected contact models – EEPA and bonded particle model – were performed.

Densely packed, randomly arranged three-dimensional spheres vary in size and shades of gray, including white and off-white.

Modeled particle bed: an EDEM-modeled NMC electrode from TU Munich, iwb, David Schreiner

Combining EEPA and bonded particle model enables a good description of the behavior of the electrode microstructure during calendering. Finally, the modeled and parameterized electrode is used to determine suitable calendering parameters and to predict the effects of individual parameters.

“TU Munich has extensive expertise in calendering and the effects on lithium-ion battery electrodes,” says Schreiner. “So far, however, for each new material system, many experiments are necessary to determine suitable process parameters. Even with the same material system but changed thickness and density, the identification of suitable process parameters results in high experimental effort and therefore high expense.”

TU Munich

LEFT TO RIGHT: Generation of NMC-particles and binder-conductive-matrix; electrode section before compaction; electrode section after compaction

Even with the same material system but changed thickness and density, the identification of suitable process parameters results in high experimental effort and therefore high expense.
David Schreiner, Research Associate, Technical University of Munich