приклад

Optimizing transfer chute by providing greater insight than using traditional design methods

Longking employs Simcenter EDEM software to reduce probability of blockages while cutting dust emissions

Longking employs Simcenter EDEM software to reduce probability of blockages while cutting dust emissions
Poorly designed transfer chutes can cause belt misalignment.

Longking

Longking Bulk Materials Science & Engineering Division is a specialized group that designs and supplies bulk handling and storage equipment to clients around the world.

https://www.longking.com.cn/

Головний офіс:
Fuijian, China
Продукти:
Simcenter EDEM
Промисловий сектор:
Industrial machinery

Поширити

Simcenter EDEM was an effective design tool to model the flow of coal through the existing design and develop a robust chute design to solve the ongoing problems. The new design has been implemented and the solution has solved the issues.
Rongfu Liao, Chief Engineer of Dust Suppression, Xiamen Longking Bulk Material Science & Engineering

About the customer

Longking is a large engineering and manufacturing company in China. Longking Bulk Materials Science & Engineering Division is a specialized group that designs and supplies bulk handling and storage equipment for clients around the world.

Simcenter™ EDEM™ software simulation technology was used to evaluate issues of blockage and dust emission of a transfer chute, and propose a new design that would solve the problem.

Their challenge

At a power plant in China, thermal coal is processed in a tall building to screen and crush oversized material. Several chutes connect the feed conveyor to the screen and crusher where sub-30-millimeter (mm) material is fed into the outgoing conveyor. The main issues that needed to be addressed in this project were:

  • Significantly control and reduce dust emission
  • Reduce likelihood of blockages occurring when handling wet coal
  • Improve loading on the outgoing conveyor
longking - feature

Our solution

Simcenter EDEM, which is part of the Siemens Xcelerator business platform of software, hardware and services, was used to run simulations of the existing design and identify flow problems with dry and wet coal. Postprocessing was conducted to evaluate coal velocity at various locations, impact velocity on the lower chute and outgoing conveyor, and the presentation of coal on the outgoing conveyor (for example, side loading). The Longking team also evaluated slip velocity between the coal discharging the lower chute and outgoing conveyor (to assess if the coal is softly loading the belts).

The data and observations from the Simcenter EDEM simulations were used to commence redesigning the lower section of the chute. Several design concepts were developed. To determine which design was optimal, Simcenter EDEM simulations were conducted to evaluate the performance of each design. The final design showed improvements including:

  • Controlled flow in spoon chute
  • Soft loading on outgoing conveyor to reduce dust emission
  • Improved velocity profile on outgoing conveyor
  • Improved central loading on outgoing conveyor

In addition, a relative wear analysis was conducted in Simcenter EDEM to examine the normal (impact) wear and tangential (abrasive) wear on the new lower chute. This analysis assisted Longking engineers in designing the wear liner package.

A black semicircle appears on a white background.

Longking used Simcenter EDEM to evaluate transfer chute design and improve efficiency.

Results

The Simcenter EDEM capability to accurately simulate the coal flow through a crushing and screening station enabled Longking to gain greater insight than using traditional design methods, and to be confident that the design would perform well with low probability of blockages while reducing dust emissions. In addition, Simcenter EDEM visualization helped Longking demonstrate the design solution to the client and increase their confidence that the solution would work to solve the issue.

“Simcenter EDEM was an effective design tool to model the flow of coal through the existing design and develop a robust chute design to solve the ongoing problems,” says Rongfu Liao, chief engineer of dust suppression, Xiamen Longking Bulk Material Science & Engineering. “The new design has been implemented and the solution has solved the issues.”