กระดาษสีขาว

Timing exceptions demystified

An abstract 3D render of a blue circuit board with many electrical components installed. The central microprocessor has an integrated LCD showing glowing binary code. Components are labelled with random serial numbers.

One of the biggest challenges in timing constraints is the usage of timing exceptions such as false and multi-cycle paths. Because the usage of these exceptions are not well understood by designers, it often results in silicon failures. Furthermore, some EDA vendors are also responsible for adding to the confusion by promoting the blind usage of exceptions in order to promote their products.

Unfortunately, timing exceptions are a necessary evil that tend to creep into every SDC file, intentionally or non-intentionally during multiple stages of the ASIC design flow. However, when understood and used properly can provide great benefit.

This paper attempts to explain the timing exceptions and their proper usage in the ASIC flow.

แบ่งปัน

แหล่งข้อมูลที่เกี่ยวข้อง