กระดาษสีขาว

Understanding die attach thermal performance for power electronics

Image of electronics with superimposed blue data to signify testing the die attach thermal performance

The goal of ON Semiconductor is to create and supply its clients with power electronic components, like wide band gap semiconductors, that perform optimally when exposed to high and low temperatures. This white paper discusses testing procedures and solutions that can be applied to prevent future device failure due to harsh temperatures.

Temperature fluctuations can result in the solder die attach breaking, the die attach delaminating from the die, or the die-attach separating from the substrate. Like a domino effect, this leads to higher temperature, which further damages the device, until complete failure.

Testing

  • Improves device performance and reliability
  • Extends the life of the product
  • Accelerates time-to-market
  • Reduces costs

Improve thermal performance with advanced testing solutions

Evaluating the effect of the voids on the thermal impedance of the die-attach, requires a highly sensitive measuring device and a method for determining the impact of the die attach on the overall measured thermal resistance

Thermal Structure Function analysis is a non-invasive way to visually find faults in the layers of a packaged device. Siemens Simcenter POWERTESTER tools measure current, voltage, and die temperature while utilizing structure function analysis to document package structure changes or defects.

Because it offers the requisite measurement accuracy, POWERTESTER 1500A was specifically utilized during testing. Coupled with the integrated structure function analysis of the Zth curve, it can determine the partial thermal impedance caused by die attach. Analysis of automatically captured data was done with Simcenter T3STER Master software.

Die attach solutions to meet unique power electronics requirements

The method employed using Simcenter POWERTESTER 1500A complies with the JEDEC JESD51-14 standard. demonstrating a non-invasive electrical test to both heat the die and detect the die temperature.

JEDEC is the industry leader for creating open standards for the microelectronics sector. Accredited by ANSI, this regulatory body ensures product compatibility, improves time-to-market and lowers product development costs for the benefit of the industry and, eventually, the consumer.

What you will learn in this die attach thermal performance paper

Follow along as ON Semiconductor:

  • Explains how the thermal performance of the package is affected by the size, location, and distribution of voids
  • Determines the most accurate method and tools for calculating the junction-to-case resistance
  • Analyzes the implications of die attach layer voids on the junction-to-case resistance
  • Measures ten samples, a through j, using the temperature versus time derivative method

Want to learn more? Download and read the whitepaper.

แบ่งปัน

แหล่งข้อมูลที่เกี่ยวข้อง