กระดาษสีขาว

Keeping one step ahead with predictive maintenance

Industrial AI and Industrial Edge

Computer control room used for predictive maintenance overlooking factory floor

Now more than ever, companies must be able to maintain and improve their overall equipment effectiveness (OEE). This is no easy task given today's challenges: companies’ expenses are rising due to the increasing cost of raw materials and skilled labor. At the same time, competitors are gaining market share faster and faster in traditional industries, and companies must be able to keep up with this pace. Effective maintenance is the key to achieving the desired OEE. This requires having the right machine maintenance procedures in place, such as predictive maintenance.

Finding the right maintenance strategy

Optimal utilization of production capacity means that production should ideally run around the clock
to take full advantage of market opportunities. The right approach for machine maintenance utilizes several strategies:

  • Prevent outages with predictive maintenance
  • Predictive maintenance based on consumption data
  • Mechanical vibration monitoring for predictive maintenance
  • Using a combination of Industrial AI and Industrial Edge

Increase machine availability

Predictive maintenance based on consumption data or mechanical condition data can already provide companies with a major competitive advantage and is often already used extensively in industry. Predictive maintenance based on an edge infrastructure and AI is the next step in extracting even more value from the data obtained. A major advantage of this standard architecture is the ability to scale a solution to multiple lines.

แบ่งปัน

แหล่งข้อมูลที่เกี่ยวข้อง