กระดาษสีขาว

Effectively addressing the challenge of securing connected and autonomous vehicles

Tessent and Secure-CAV ensuring a future of cybersecure connected vehicles.

Vehicles are becoming the most sophisticated connected objects in the ‘Internet of Things’. As vehicles integrate functionality that will enable a fully autonomous future, the attack surface grows substantially. Combined with remote connectivity at multiple points, the clock is ticking in a race to improve cybersecurity in all types of vehicles to ensure that all stakeholders, but particularly drivers and passengers, can have full confidence that future Connected and Autonomous Vehicles (CAVs) are both safe and secure.

The automotive industry has a challenge in that legacy technologies are both insecure and take a long time to age-out. Unlike many other connected products, vehicles can have a very long lifespan, which demands an innovative approach when it comes to cybersecurity concerns.

The Innovate UK-sponsored Secure-CAV consortium set out to develop and prove hardware-based security technology that will allow the automotive industry to leap ahead of the threats that it faces currently and in the near-term, putting the industry into a much more tenable cybersecurity posture than it currently holds.

Siemens has developed Intellectual Property (IP) as well as anomaly detection software, which is able to monitor protocols and transactions at the lowest level in hardware. This is backed by unsupervised machine learning algorithms and statistical analysis, with expert input from the University of Southampton. This was integrated into Field-Programmable Gate Array (FPGA) technology and linked to two vehicle demonstrators developed by teams at Coventry University and cybersecurity specialists Copper Horse. A range of selected real-world threats were exercised, including purchasing and analyzing hacking equipment for existing vehicles.

แบ่งปัน

แหล่งข้อมูลที่เกี่ยวข้อง