วิดีโอ

Multiphysics Engineering Solution

Intelligent Performance Engineering (IPE) is a comprehensive engineering solution designed to help industrial machine manufacturers manage the complexities of building the next generation of machines with lower costs and fewer risks.

This integrated design solution places multiphysics simulation, integrated design, and simulation, and closed-loop validation in the same digital environment.

With all those tools in a single location, teams can more easily connect, allowing designers and engineers to collaborate more efficiently.

Benefits of multiphysics simulation

Multiphysics simulation brings together a wide range of physics disciplines under one umbrella.

Engineers can capture complexities and address multiple needs at the same time as they study phenomena across physics domains.

Structural, thermal, fluid flow and electromagnetic interactions in a single simulation give engineers a better understanding of how a machine will operate, and it can be achieved earlier in the development process.

Design and simulation engineering collaboration

Integrated design and simulation connect designers and simulation engineers to the same models in one system.

When simulation data stays in sync with design, it increases efficiency and improves collaboration across disciplines.

The digital twin simulates and validates designs virtually, allowing machine builders and equipment manufacturers to find and fix issues earlier in the process, which reduces costs, lowers risks, and increases machine reliability.

Validate simulation with closed-loop validation

Closed-loop validation leverages the IIoT to validate simulations by capturing data from the field.

That same data is then used as an input to test the relationships between requirements, functional layouts, logical implementation, and physical implementation.

All of this can then be used to improve the engineering and design of current and future machines to better meet the growing demands of customers.

Multiphysics simulation software

Leverage Siemens multiphysics engineering solutions and simulation to improve manufacturing and plant processes and drive innovation with team collaboration.

แบ่งปัน

แหล่งข้อมูลที่เกี่ยวข้อง