Teknisk papir

Reduce the time delay between P&R and physical verification

Reduce the time delay between P&R and physical verification

Using a P&R tool’s built-in fill function to place filler cells during implementation is not only time-consuming, but can create layouts that do not comply with design requirements. The Calibre YieldEnhancer PVReady flow ensures correct-by-construction filler cell, DCAP, and ECO cell insertion during P&R in less time, using standard industry interfaces that seamlessly integrate with both the P&R and physical verification tools. In addition, because filler cells must be replaced throughout the design process, the runtime reductions are additive, which can significantly reduce time to tapeout.

Dele

Relaterte ressurser