백서

Expediting simulation turnaround time with incremental build flows

At the sub-system level, a lump sum build approach may be all you ever need.

 Expediting simulation turnaround time with incremental build flows | A lump sum build is the simplest build approach. All the inputs into one bucket; that bucket of stuff compiled into one library.

Rapid simulation turn-around time is critical for high-functioning SoC teams because it enables a tight feedback cycle that teams use to constantly validate progress. A big part of enabling that rapid turn-around time is a fast and effective build flow. This paper walks the reader through a few of those options; starting with a simple lump sum build and working through options that enable an optimal SoC build flow.

The Optimal SoC Build Flow

Whether the result is a failed compile, passing simulation, or anything in between, the sooner you get that result, the sooner you get to the next step and closer you get to your ultimate objective: passing silicon. Questa has a few different options for optimizing build flows depending on the application. This paper describes a few of those options, starting with a simple lump sum build and working through simulation options that enable an optimal SoC build flow.

Questa users have a lot of flexibility when it comes to finding the build flow that’s right for them. Whether you’re verifying a small sub-system as a one-person team or an entire SoC with a much larger team, the combination of compiled library partitioning, PDUs, parallelism and elaboration
flow are the tools you need for an optimal build flow and reduced SoC build times.

공유

관련 자료

Operational SVA의 타이밍 다이어그램 캡처
White Paper

Operational SVA의 타이밍 다이어그램 캡처

이 글에서는 타이밍 다이어그램과 파형에서 손쉽게 속성을 도출하기 위해 필요한 언어 구조를 제시하고, 이것이 Siemens EDA의 Operational SVA에서 어떻게 구현되는지를 제시합니다.