White paper

High-Level Synthesis, it’s still hardware design

High-Level Synthesis, It’s Still Hardware Design: 3d illustration of futuristic microchip city.

This paper talks about who the key individuals are that need to be involved in a successful High-Level Synthesis (HLS) hardware design flow and the challenges of designing using HLS.

Who are the key players for successful HLS design flow

Hardware design using HLS is no different than the typical ASIC/FPGA design flow with the exception that C++/SystemC is being used along with HLS to create the RTL instead of hand coding it. The advantage of using HLS is that it speeds up RTL creation time and reduces verification time by producing bug free RTL quickly from a fully verified C++/SystemC source. The misconception that still exists today is that anyone can design using HLS to create optimal hardware. The reality is that you still need to involve all of the people in a typical hardware design flow including the algorithm engineers, the hardware/system architects, and the RTL designers if the expectation is to achieve results as good or better than hand-coded RTL.

Hardware design is hard

Not anyone can do hardware design using HLS for production ASIC/FPGA that is efficient for power, performance, and area (PPA). If this was true there would be no need for hardware/system architects or RTL designers. In fact, hardware design requires an in-depth understanding of memory architecture, concurrent processes, and optimization of algorithms running in software to create efficient implementations running in hardware.

Condividi

Risorse correlate

Un produttore di aerei utilizza le soluzioni Siemens per ridurre i tempi di sviluppo dei prodotti per gli aeromobili in materiali compositi completamente elettrici
Case Study

Un produttore di aerei utilizza le soluzioni Siemens per ridurre i tempi di sviluppo dei prodotti per gli aeromobili in materiali compositi completamente elettrici

NX, Fibersim e Simcenter migliorano la produttività di Bye Aerospace con il 66% di personale tecnico in meno

Potenza e flessibilità senza precedenti con il CAD cloud-native
White Paper

Potenza e flessibilità senza precedenti con il CAD cloud-native

Aumenta l'efficienza della progettazione elettrica e la collaborazione con Capital Electra X, il software CAD cloud-native di Siemens. Scopri di più