livre blanc

Including electrothermal effects in electronics design with connected FANTASTIC BCI-ROMs

Temps de lecture : 13 minutes
Schematic drawing of thermal connections and inputs for a two-heat source, two ambient face BCI-ROM

The coupling of thermophysical properties, power dissipation, and temperature are difficult to consider early in the design process. To address these issues, accurate thermal capabilities must be introduced early in design areas. To bridge this divide, this work illustrates how to leverage the FANTASTIC reduced order model (ROM) extraction methodology to convert 3D thermal simulation models into BCI-ROMs in the VHDL-AMS format and then connect them to form accurate electrothermal circuits using 1D tools.

Partager

Ressources connexes