aperçu de la technologie

Supply Chain Resilience with PADS Professional Premium

Durée de visionnement estimée : 2 minutes

When creating a schematic, the Supply Chain cloud application, which is integrated directly within the schematic tool, provides engineers with real-time component sourcing data, empowering them to make informed decisions about their selected components when the cost of making changes is lowest.

Supply Chain Resilience

Supply Chain is powered by Siemens Supplyframe and is connected to more than 80 suppliers, world- wide, providing access to component information, including:

  • Pricing
  • Compliance
  • Availability
  • Lifecycle data

Visual indicators are present in the part list, so when you are filtering or sorting parts, all it takes is a quick visual inspection to identify potential issues. This allows you to spend less time searching and sourcing components and more time innovating. To create a bill of materials based on the suppliers and manufacturers you’ve chosen, an Excel export file can be generated using the customizable view you can create in Supply Chain.

Learn more about PADS Professional Premium.

Partager

Ressources connexes