étude de cas

ROHM speeds automotive product development by adopting PartQuest Promote from Siemens

ROHM improves customer engagements, lowers time-to-volume, and enables easy verification of solution circuits by incorporating Siemens’ PartQuest Promote into its cutting-edge web simulation tool

ROHM speeds automotive product development by adopting PartQuest Promote from Siemens
Ippei Yasutake and a team member evaluating the ROHM Solution Simulator

ROHM

Semiconductor and electronic components manufacturer

https://www.rohm.com/

Quartiers généraux:
Kyoto, Japan
Secteur de l'industrie:
Electronics, Semiconductor devices

Partager

We chose Siemens’ PartQuest Promote platform because it is the only solution that meets all of our requirements.
Ippei Yasutake, Group Leader of Solutions Engineering, ROHM

Headquartered in Kyoto, Japan since 1958, ROHM Co., Ltd. is a global semiconductor and electronic components manufacturer. In the early 1970s, ROHM led the expansion of Japanese high-tech companies into the U.S. and other foreign markets and maintains its leadership with persistent investment in modernization and with factories, sales offices, and technical centers around the world.

Today, ROHM is renowned for its wide product lineup, featuring excellent performance
and reliability. ROHM has made great contributions to energy saving, miniaturization,
and design load reductions in applications. In the power field, they were the first in the
industry to commercialize the next-generation power device, SiC MOSFET. In the analog field, they have introduced leading-edge technologies such as the innovative power supply technology “Nano” series and the high noise tolerance amplifiers/comparators in the “EMARMOUR” series.

In addition to driver ICs that maximize power device performance, ROHM is focused on solving customer issues with high-quality, targeted solutions and support tools. Their vertically integrated production system, from wafer manufacturing to circuit design, packaging and testing, ensures a long-term stable supply of products and reliability based on thorough traceability.

The best ingredients are more than SPICE

Automotive OEMs and Tier 1 companies are among ROHM’s key customers. They need functional verification using simulation and analysis to ensure the time- to-market, quality, reliability, and
safety requirements of circuits and models they develop using model-based design. ROHM customers in other industries have similar needs due to model based design becoming a wide- spread practice.

Simulation is so important for model-based design because it reduces the time and effort of component selection and identifies potential or fundamental issues before physical product validation. Additionally, in the design of electronic circuit boards, simulation significantly decreases time and effort during the board proto-typing and evaluation phases.

Previously, ROHM used only SPICE simulation models to tune their components to their customers’ specifications. In turn, their customers downloaded these SPICE models to use in their own SPICE simulation environments.

However, SPICE models present several problems. There is no definitive SPICE standard, making it impractical if not impossible to offer a single, universal model that works in every customer’s
SPICE simulator-of-choice.

Conversely, providing a different model for every type of simulator is prohibitively expensive. And, importantly, SPICE models predict only electrical performance, while automotive suppliers need to verify broader characteristics, particularly for thermal behavior, which presents many trouble spots in application design.

Therefore, to overcome the limitations of conventional SPICE models, the Solutions Engineering department within the Application Engineer Division at ROHM wanted to offer an innovative, online simulation environment that would help their customers more quickly select, integrate, and validate ROHM components. The ability to provide such a solution not only fulfills ROHM’s “Quality First” mandate but also helps them propose the best components for their customers’ designs.

“We felt that effective application design needs an easy-to-use environment to conveniently and fully simulate our proposed circuits online,” recalls Kunihiro Komiya, Manager of Solutions Engineering department at ROHM.

Understandably, the ROHM team wanted to accelerate the introduction of this more versatile and easier-to-use online simulator environment. So instead of creating an entirely new solution from scratch they looked for an existing platform they could build upon.

After careful consideration of the options, the ROHM team determined that only the PartQuest™ software Promote platform from Siemens offered the features they were looking for. This unique set of features includes:

  • A multi-domain simulator that supports
    model-based development
  • Support for SPICE and VHDL-AMS models
  • Straightforward expansion to thermal
    simulation
  • ROHM customer cloud simulation hosted
    on ROHM’s website
  • Cost-effective, self-service registration
    of ROHM components as libraries in the
    technology design platform utilized by
    PartQuest Promote.
  • Recommendation by the Society of
    Automotive Engineers of Japan, Inc.,
    supporting ROHM’s strategy to focus on
    automotive market
  • Accelerated simulation using highly
    abstract models, especially important
    when simulating a solution circuit with
    multiple ROHM components
  • Support from Siemens application
    engineers

“We chose Siemens’ PartQuest Promote platform because it is the only solution that meets all of our requirements,” explains Ippei Yasutake, Group Leader of Solutions Engineering department at ROHM.

The best platform for cloud based simulation

PartQuest Promote is a cloud-based software service provided by Siemens that allows users to perform the latest multi-do-main simulations. This system, which can be accessed from a web browser to carry out analysis anytime, anywhere, supports encrypted VHDL/AMS and SPICE models. Because the circuit topology can be imported from PartQuest Promote’s simulation environment into Xpedition, Siemens’ flagship PCB design tool, customer designs can be smoothly connected to the PCB board design flow.

PartQuest Promote enables ROHM customers to exercise “executable specifications” within a cloud environment. Adopters can easily change circuit design parameters in the cloud without the time and expense of test equipment.

This solution encourages ROHM’s customers to achieve optimal device configuration.

Importantly for ROHM’s automotive customers, the PartQuest Promote simulator can handle not only electric circuits but also mechanical and thermal circuit models. In addition, it has superb usability characteristics, including circuit diagram creation, graphical wave-form display, and tunable design operation (i.e., fixed-topology circuits with tunable design choices that can be embedded and simulated directly on the ROHM website). These all add-up to a solution that make ROHM parts the quick and easy choice for circuit designers.

“PartQuest Promote enabled us to quickly deliver our high-quality, cloud-based simulation environment,” Makoto Terada, Group Leader of Solutions Engineering department at ROHM reports.

By building upon the PartQuest Promote platform, ROHM was able to speed the development of its cutting-edge, web-based simulator, the ROHM Solution Simulator. This cloud-based simulation environment allows users to perform complete circuit verification of power devices and driver ICs at the same time, making it possible to quickly and easily validate ICs along with power devices under close-to-actual conditions.

A person is standing in front of a white wall with a blue and white logo on it.

ROHM Solution Simulator GUI

“Leveraging the feature of being able to simulate in a cloud environment, we embedded the PartQuest Promote system on our official website and started to provide a web simulation tool, the ROHM Solution Simulator in early 2020,” explains Kunihiro Komiya. “This platform enables customers to simulate power devices, driver ICs, and power supply ICs on a solution circuit together.”

These capabilities allow electronic circuit designers and system designers to significantly reduce the number of application development steps and prevent problems before they occur.

“While solving the problems associated with SPICE models, our new solution simulator allows our customers to not only reduce the development time required to select components, but also reduce circuit design issues by tuning and testing their circuits virtually,” says Kunihiro Komiya. “Customer response has been tremendous!”

Because PartQuest Promote enables ROHM customers to simulate in a cloud environment hosted on ROHM’s website, ROHM is now able to respond to customers’ need for simulation, increase the inflow of engagements to ROHM’s website, and deliver the latest product information directly to its customers.

But it doesn’t stop there. Because the ROHM Solution Simulator is built on PartQuest Promote, it is easy for circuit designers to leverage the ROHM-provided circuits by seamlessly migrating their design work to the PartQuest Explore application that services the product
design community. ROHM customers can use their personal PartQuest Explore accounts or take advantage of collaboration groups sponsored by ROHM on the PartQuest Explore site. In online groups, ROHM application engineers can engage in design iteration directly (and privately) with customers, ensuring customer success with ROHM components.

“Now we can focus on maintaining a single, standardized set of device models and reference circuits,” says Kunihiro Komiya. “With PartQuest Promote’s online collaboration features, we can amplify our customer engagement at a fraction of the cost of onsite visits.”

Supported by PartQuest Promote’s online tools, including simulation, ROHM plans to continue to add solution circuits and products, including models for thermal simulation, to the component libraries supported by the ROHM Solution Simulator and PartQuest Promote platforms.

“We are going to increase our circuit lineup so that we can provide even more customer value, and we already see more customers making more use of PartQuest Promote and our ROHM Solution Simulator as they run simulations again and again by changing component values,” Ippei Yasutake observes. “Most importantly, we believe we will achieve a reduction in customer circuit verification time and circuit design errors.”

“It’s great to be able to provide this simulation service on the ROHM official website!” Makoto Terada concludes.

Person in black shirt standing against a black and white patterned wall, holding a dark object.

Using the ROHM Solution Simulator