valge paber

Root cause deconvolution: The next step in scan diagnosis resolution

RCD results from 28nm yield ramp

Root Cause Deconvolution (RCD) dramatically improves scan test diagnosis resolution by analyzing multiple layout-aware diagnosis reports together to identify the underlying defect distribution (root cause distribution) that is most likely to explain this set of diagnosis results. The results are then back-annotated to the individual diagnosis suspects. Where layout-aware diagnosis points to a segment, RCD can isolate a particular root cause in that segment. This increase in the relevance and success rate of failure analysis (FA) and dramatically reduces the FA cycle time from months to days.

Scan logic diagnosis turns failing test cycles into valuable data

Scan diagnosis is an established method to locate defects in digital circuits. The quality of diagnosis results is measured using two metrics; accuracy and resolution. Accuracy is a measurement of whether the diagnosis result contains the actual defect or not. Resolution measures the area of the defective location captured by a suspect. The area is a bounding box of a defect and the length of the list of candidates. More candidates leads to more bounding boxes and more search area. Thus, in general, a shorter list of candidates has a better resolution than a longer list.

However, diagnosis results contain ambiguity, or noise, in the diagnosis that limits the resolution. RCD eliminates the noise from the diagnosis results and determines the underlying root causes represented in a population of failing devices.

This paper describes the challenges of scan diagnosis resolution, the benefits of applying the RCD statistical method, plus a more detailed description of how it works and examples from published results of real world case studies.

Jaga

Seotud ressursid