valge paber

Comprehensive statistical analysis of SERDES links considering the effect of DFE error propagation

Solution flow that is based on the step response

As signal rates increase and link behavior becomes marginal, DFE error propagation cannot be ignored. However, time domain simulation becomes impractical for the error probabilities as low as 1e-15, while existing statistical simulation methods cannot properly consider DFE feedback that may contain errors. The methods known today combine the elements of statistical analysis and combina-torial approaches to find probability of errors following specific combinations of symbols and DFE taps. They have exponential time complexity which prevents from using them in general-purpose link simulators. We propose statistical approach which seamlessly includes DFE into computational loop and provides required performance without simplifications.

Introduction and overview

As the speed of digital transmission increases, the links operate at their margins defined by the
channel loss, reflections, jitter, crosstalk, noise and other impairments. For this reason, designers use all available equalization schemes to improve the signal to noise ratio at the receiver output. DFE (decision feedback equalizer) is one of the important equalization instruments. Unlike linear equalization (FFE and CTLE), it provides a feedback signal to eliminate inter-symbol interference associated with already
detected symbols. However, if the detected symbol
is wrong, the feedback is no longer the desired
signal, and it can increase the probability of subsequent errors. This leads to so-called DFE error propagation or burst error.

The paper is organized as follows. Sections II-IV
define the essential building blocks of the statistical solver. In section II we provide definitions of the
main elements of the statistical analysis and
compare the single bit/pulse response-based
approach with the incremental transitions approach. Section III introduces the “convolution term”, the
new element of the statistical solver that includes various types of DFE feedback. Section IV defines symbol error probability matrix and its use when building statistical convolution terms. The flow that finds the BER/SER metrics of the channels in presence of DFE error by iterations is defined in section
V. Section VI discusses the use of the modified
iteration process to find the probability distribution of symbol error groups, and section VII describes the experimental study of the statistical solver.

Jaga

Seotud ressursid