valge paber

A Stroke Of Genius: Saving Time And Effort With Sketch Routing

A Stroke Of Genius: Saving Time And Effort With Sketch Routing

As designs increase in complexity, it becomes much more difficult to create and maintain design rules that will offer the results that an experienced designer can achieve routing manually. Some reasons that designers have for shunning autorouting include:

• The intimidation factor of trying to set up the autorouter in a way that will translate the designer’s vision to the screen

• Reduction in quality versus a hand-drawn design

• Time spent cleaning up after the autorouter could have been spent manually routing it in the first place

• Too many vias – or, the general inability of an autorouter to complete a design with the elegance that an experienced designer could.

Manual routing vs. automatic routing

Both autorouting and manual routing require careful planning strategies and execution to achieve ideal results. Generally, the best autorouting success is accomplished when the design team has dedicated time to plan, place, constrain and prioritize the design database with autorouting in mind. Autorouting success is also determined by the designer’s knowledge of their autorouter’s algorithms and historical performance.

How does sketch routing work?

To use sketch routing, the designer simply draws a line to dictate the path around which the selected netlines should be routed. The sketch router can route individual, dozens, or even hundreds of netlines many times faster than manual routing. In figure 3, twenty-two data lines have been selected. The most common method of sketch routing uses the existing via fan-outs and does not add any additional vias.

This paper explains automation in PCB design software which lets engineers create more complex designs at an increased rate.

Learn more about PADS Professional Routing Automation.

Jaga

Seotud ressursid