e-book

Descubra cómo NX está potenciando la tecnología generativa

Tiempo de lectura: 18 minutos
Descubra cómo NX está potenciando la tecnología generativa

En el último e-book de CIMdata, descubra cómo NX está liderando el camino de la tecnología generativa.

Con este e-book obtendrá más información sobre:

  • Nuevos métodos de diseño como optimización de la topología y modelado convergente
  • Todo sobre diseño generativo
  • El ciclo iterativo
  • Ejemplos de diseño generativo

Con las últimas innovaciones de NX en diseño de producto, CIMdata le enseña cómo beneficiarse de lo que puede hacer para crear productos más ligeros y potentes con los nuevos métodos que se encuentran en el e-book.


Explore more design options in less time with generative design

Generative design is turning the traditional design paradigm on its head. Conventional design methods rely on a "model then analyze" iterative cycle, but in generative design, the product designer first identifies the necessary design space and design goals. Once initialized, software algorithms do the job of automatically cycling through numerous geometric model permutations seeking an optimum solution based on defined constraints without the need for human intervention. Generative design methods facilitate faster decision-making, and with a given set of conditions, designers can conduct more experiments in much less time than is possible with traditional design methods.

Minimize cost and optimize performance with generative technology

The emerging technology of generative design is gaining interest in product development communities because it creates optimized product designs from requirements and constraints rather than by making the geometry first and then validating. Designs are optimized to objectives like minimum cost and weight when using physics-based simulation and other analysis methods that consider performance requirements. This approach reduces material waste and cost by creating models that require only the material amount needed to meet product requirements.

Utilize topology optimization to reduce material use

The most recognized generative design process is topology optimization. It optimizes material layout within given design spaces for a set of functional requirements, including loads, boundary conditions, and constraints. Typically, the optimization goal is to meet the model's structural strength while minimizing its mass, thereby reducing its weight while saving on material. While most implementations are in prototype study or one-off parts, the future will bring more examples staged in a production environment. Although the future direction is uncertain, Siemens NX software has set the fundamental first stage to support their customers' generative design journey no matter which direction that journey will take.

Compartir

Recursos relacionados

Diseño de nueva generación para automoción y transporte
Webinar

Diseño de nueva generación para automoción y transporte

Siemens ofrece una innovadora herramienta de diseño que cambiará el sector.

Diseño óptimo a la primera gracias al codiseño ECAD-MCAD en automoción
White Paper

Diseño óptimo a la primera gracias al codiseño ECAD-MCAD en automoción

ECAD-MCAD con la mayor probabilidad de éxito a la primera para seguir siendo competitivas. Descubre cómo integrar aún más el dominio eléctrico y el mecánico.

El coche del futuro: Eléctrico, conectado y autónomo, por Joe Barkai
White Paper

El coche del futuro: Eléctrico, conectado y autónomo, por Joe Barkai

Descubra cómo los vehículos del futuro cambiarán el mercado de proveedores a través de la integración electromecánica y los diseños más ligeros.