white paper

Concepts of signal integrity: crosstalk

Concepts of Signal Integrity: Crosstalk

Crosstalk crops up in every design. It is one of the most common signal integrity issues that engineers have to deal with. This paper, the third in our series on the concepts of signal integrity, explores the essential principles of crosstalk and what you can do to reduce it.

Two phenomena's of coupling

This paper explains that coupling can happen through two phenomena: capacitive and inductive noise. Because of that, only the switching edge of a signal will contribute
to coupling whereas the steady state section will not. Once a signal couples onto a victim net, the noise will propagate in both directions. The signature of a near-end crosstalk is a wide pulse, whereas the electrical signature of a far-end crosstalk is a narrow pulse. Also shown in this paper is that the biggest noise contributors are the closest aggressors to a victim net.

Essential principles of crosstalk and what you can do to reduce it

Crosstalk is a signal integrity issue that occurs when the signal from one trace couples with another trace, causing interference. There are three essential principles of crosstalk: capacitive coupling, inductive coupling, and conductive coupling.

The first two are the most common and occur when the signal from one trace couples with the signal from another trace through either a capacitor or an inductor. Conductive coupling, on the other hand, occurs when the signal from one trace couples with the signal return path of another trace.

Crosstalk can be controlled by using proper signal routing techniques, impedance control, and shielding. By understanding these principles and utilizing these mitigation techniques, you can help to ensure signal integrity in your designs.

Learn more about Signal Integrity.

Share

Related resources

SLEC System Factsheet
Fact Sheet

SLEC System Factsheet

SLEC System is a good fit for design teams verifying their RTL implementation by formally comparing it against functional SystemC/C++ models

Catapult High-Level Synthesis and Verification Fact Sheet
Fact Sheet

Catapult High-Level Synthesis and Verification Fact Sheet

Industry leading C++/SystemC High-Level Synthesis with Low-Power estimation/optimization. Design checking, code and functional coverage verification plus formal make HLS more than mere “C to RTL.

DVCon 2025:  A must for hardware design and verification engineers
Blog Post

DVCon 2025: A must for hardware design and verification engineers

I've attended every DVCon US conference since its inception, over 30 years ago. I've also given keynotes at DVCon India.…