white paper

Achieving functional safety for autonomous vehicle SoC designs

Design for safety analysis.

Achieving functional safety for autonomous vehicle SoC designs

Vehicle architecture design is converging to a more centralized, domain-processing model. These domain-based processors are the new key differentiator for car buyers. Domains such as automated driving, vehicle connectivity and mobility solutions that rely on sophisticated AI algorithms and intense computations require SoCs optimized for the specific challenges of each application. Ensuring safe operation of these complex SoCs is a monumental task guided by ISO 26262 and SOTIF. This paper details some of the fundamental activities and concepts in achieving that goal.

Despite the numerous challenges involved in designing SoCs for autonomous vehicles, the most substantial obstacle to their success is earning the trust of the public. One way autonomous vehicle (AV) manufacturers can establish this trust is to demonstrate the safety and reliability of their platform through safety standards and certification. To that end, the automotive industry has established a set of procedures and standards focused on the safety of electrical and electronic systems, known

as functional safety.

The goal of functional safety is to reduce the risk of electrical and electronic components malfunctioning due to failures. In the automotive industry, these procedures and requirements have been formalized in the ISO 26262 standard. ISO 26262 requires that electronics be tested for random hardware failures and systematic faults. ISO 26262 is also the technical state of the art for automotive electronics safety, making compliance essential for automotive manufacturers and suppliers that release products susceptible to liability suits.

Systematic faults are those that prevent an integrated circuit from operating correctly according to the product specifications. These could be design bugs, hardware/software interface problems, misinterpreted or incomplete specifications and so forth. The IC industry has accrued a lot of knowledge, tools, and processes for dealing with systematic faults. In comparison, the industry is less experienced and not as well-equipped for finding and resolving random hardware faults. Random hardware faults are unpredictable and occur over time as the IC operates.

Share

Related resources

Are you safe yet? Safety mechanism insertion and validation
White Paper

Are you safe yet? Safety mechanism insertion and validation

As functional safety becomes increasingly important in today's industrial and automotive designs, many legacy designs have to be “upgraded” to meet the safety goal of the system.

Push-button FMEDAs for automotive safety — automating a tedious task
White Paper

Push-button FMEDAs for automotive safety — automating a tedious task

Automotive designs require functional safety analysis, typically accomplished using Failure Modes, Effects and Diagnostic Analysis (FMEDA), used to determine each safety goal’s diagnostic coverage.

Orchestrating an efficient ISO 26262 fault campaign
White Paper

Orchestrating an efficient ISO 26262 fault campaign

This paper details the methodology and tools required to accelerate and close on an ISO 26262 fault campaign