White Paper

Assuring the integrity of RISC-V cores and SoCs

GapFree Verification Process

Assuring the integrity of RISC-V cores and SoCs

The open RISC-V processor architecture is shaking up the intellectual property (IP) and system-on-chip (SoC) worlds. There is great interest and much industry activity underway. However, successful RISC-V core providers will have to verify all aspects of integrity for their designs: functional correctness, safety, security, and trust. SOC developers evaluating potential RISC-V need to check that their standards for design integrity are fully satisfied. They may wish to re-run the core-level verification steps and then perform additional tasks to ensure that the cores have been integrated properly. Verification of RISC-V designs is especially challenging because of optional features, implementation flexibility, and provisions for customer extensions.

This paper presents the Siemens EDA RISC-V Integrity Verification solution and discussed how its components verify all four aspects of design integrity at both the processor core and full- chip levels. It concludes by detailing some issues found by the Siemens EDA solution on RISC-V core and SoC designs available as open source.

RISC-V background

Like previous generations of reduced instruction set computer (RISC) designs, RISC-V has its roots in academia. The project to develop a fifth-generation RISC- based instruction set architecture (ISA) began in 2010 in the EECS Department at the University of California at Berkeley. As with previous RISC projects both academic and commercial, the goal was to
define an ISA enabling small, fast designs with the potential for low-power operation when needed. Unlike some of those other projects, the intent was for RISC-V to support a wide variety of diverse implementations. This required the ISA to have the flexibility to map to many different microarchitectures with different power, performance, and area (PPA) tradeoffs appropriate for targeted end applications.

In 2015, the RISC-V Foundation was established to own, maintain, and publish the ISA and related documents. The original RISC-V authors and developers surrendered their rights to the foundation. There are now nearly 250 members, spanning universities, semiconductor suppliers, system houses, software vendors, and IP providers. The Foundation ensures that RISC-V remains open as per the original vision of its developers. This openness is a sharp contrast to the proprietary ISAs that have dominated computing for decades and has at least
three dimensions. First, the RISC-V ISA has been developed and evolved by a wide circle of collaborators from both industry and academia. Anyone can contribute ideas and participate in the discussions, although the ability to vote is reserved for members of the Foundation, which anyone can join.

Teilen

Verwandte Ressourcen

Flugzeughersteller nutzt Lösungen von Siemens, um die Produktentwicklungszeit für vollelektrische Flugzeuge aus Verbundwerkstoffen zu reduzieren
Case Study

Flugzeughersteller nutzt Lösungen von Siemens, um die Produktentwicklungszeit für vollelektrische Flugzeuge aus Verbundwerkstoffen zu reduzieren

NX, Fibersim und Simcenter steigern die Produktivität von Bye Aerospace durch Personaleinsparung von 66 Prozent im Konstruktionsbereich

Profitieren Sie von unübertroffener Leistung und Flexibilität mit cloudnativem CAD
White Paper

Profitieren Sie von unübertroffener Leistung und Flexibilität mit cloudnativem CAD

Steigern Sie die Effizienz der elektrischen Konstruktion und Zusammenarbeit mit Capital Electra X, der cloudnativen CAD-Software von Siemens. Mehr erfahren.