Технически документ

Bulletproof signals: Master net shielding for RF and analog designs using Calibre PERC

Simple graphic showing the net shielding concept in which a signal wire is shielded from electromagnetic effects by power or ground wires placed on either side of the signal wire.

Analog and RF circuit designs face significant challenges due to their sensitivity to various factors, including noise coupling between interconnects. One of the critical issues is the impact of proximity effects, such as crosstalk and electromagnetic interference, which can degrade the performance and reliability of these sensitive circuits.

To address this challenge, we describe the use of net shielding as an effective technique to mitigate the impact of noise on critical analog and RF signals. Surrounding sensitive signal nets with power or ground nets can create a shielding effect that isolates the signals from external interference. Calibre PERC's automated net shielding verification capabilities let designers quickly and reliably validate the effectiveness of their net shielding implementation, streamlining the design validation process and enhancing the overall reliability of analog and RF circuits.

What you’ll learn:

  • The challenges of noise coupling and proximity effects in analog and RF circuit designs, and how they can degrade the performance and reliability of these sensitive circuits.
  • The net shielding technique, which involves surrounding critical signal nets with power or ground nets to create a shielding effect that mitigates the impact of electromagnetic interference and crosstalk.
  • The benefits of using Calibre PERC's automated net shielding verification capabilities, which allow designers to quickly and easily validate the effectiveness of their net shielding implementation, saving time and effort while improving the reliability of their analog and RF designs.

Who should read this:

  • Analog circuit designers
  • RF circuit designers
  • Reliability engineers working on analog and RF designs

Сподели

Свързани ресурси