проучване на казусите

Creating a user-friendly optimization environment for defining an e-motor platform design problem

ZF uses Simcenter E-Motor Director to develop an optimization engine for building modular motor platforms

ZF uses Simcenter E-Motor Director to develop an optimization engine for building modular motor platforms

ZF

ZF is a global technology company supplying systems for passenger cars, commercial vehicles and industrial technology, enabling the next generation of mobility.

https://www.zf.com/mobile/en/homepage/homepage.html

Щаб:
Friedrichshafen, Germany
Продукти:
Simcenter E-Motor Director
Сектор на промишлеността:
Automotive & transportation

Сподели

The ability to systematically and optimally develop modular motor platforms from the ground up allows us to incorporate synergies and a common parts approach from the outset, resulting in flexible system solutions that are not simply technically advanced but also highly cost-effective.
Dr. Helmut Behm, ZF

About the customer

ZF is a global technology company supplying systems for passenger cars, commercial vehicles and industrial technology, enabling the next generation of mobility. ZF allows vehicles to see, think and act. In the four technology domains of vehicle motion control, integrated safety, automated driving and electric mobility, ZF offers comprehensive product and software solutions for established vehicle manufacturers and newly emerging transport and mobility service providers. ZF electrifies a wide range of vehicle types. With its products, the company contributes to reducing emissions, protecting the climate and enhancing safe mobility.

A vehicle chassis and undercarriage with suspension, wheels, and braking components is shown against a white background.

Their challenge

ZF develops a variety of e-motors and e-drives for a broad spectrum of automotive customers. To optimally incorporate development and production costs from the outset, their designers must find solutions to maximize shared parts within the given requirements for the motors. To achieve this, ZF groups products into motor programs that have similar design and production objectives and identifies common design features that can be used across a modular motor platform. However, the potential scope of motor configurations is extensive. With a theoretically infinite number of motor configuration possibilities, it would be impossible with only human resources to manually select an optimal combination of configurations for a motor platform while accounting for all requirements. Consequently, ZF needed a simulation and data-driven solution that would empower them to consider shared parts, costs and further constraints to automatically find the best configurations for a modular motor platform.

Diagram shows Motor 1–3, database, DOE, test scenarios, design space, optimization, and optimal concept and shape.

Modular motor platform optimization.

Our solution

Looking for a pioneering solution for the complex design optimization challenge, ZF partnered with Siemens to implement a data-driven development and optimization strategy for e-motors. Siemens is collaborating with leading global automakers to develop the Simcenter™ E-Motor Director software, which is part of the Siemens Xcelerator business platform of software, hardware and services. This highly automated environment is designed to accelerate e-motor development by facilitating multiphysics simulation, rapid design exploration and optimization based on one or multiple design of experiment (DOE) analyses.

“The ability to systematically and optimally develop modular motor platforms from the ground up allows us to incorporate synergies and a common parts approach from the outset, resulting in flexible system solutions that are not simply technically advanced but also highly cost-effective,” says Dr. Helmut Behm, ZF.

Virtual design exploration and optimization of individual designs are commonplace among motor developers but performing multi-concept and motor platform optimization brings an entirely new set of challenges. With theoretically infinite attribute combinations and multiple objective and subjective design constraints within each motor configuration, the optimization engine in Simcenter E-Motor Director needed to accommodate a flexible definition of the design optimization problem., This included defining shared and individual motor parameter settings, design variables and requirements for all members of a motor platform. All these input options and restrictions needed to be presented to the user of Simcenter E-Motor Director in a logical and intuitive user experience, giving them a clear overview of the project combined with the flexibility to adjust throughout the development process.

A mechanical device with gears and bolts sits in a casing, with a shaft passing through it.

Modular motor platform optimization.

Results

The results of the ZF and Siemens collaboration is a user-friendly optimization environment capable of handling the complex definition of an e-motor platform design problem. The environment allows the selection of an arbitrary number of reduced-order models (ROMs) to be considered and provides real-time feedback on potential ROMs that might contain possible solutions for each motor of the motor platform. Parameters and requirements can easily be set for each motor individually or linked between two or more motors of the platform. Optimizing a motor platform yields several feasible scenarios. Afterwards, the user can make a suitable selection from these possible solutions.

A grey metal device has orange wires associated with metallic components and a green component near the top on white.

Modular designed electric axle drive with integrated power electronics.